Calculate the number of consecutive characters at the beginning of a string that are contained in a set of characters.
Include
<string.h>
Prototype
size_t strspn(const char *s1, const char
*s2);
Arguments
s1 | |
s2 |
Return Value
Returns the number of consecutive characters from the beginning of
s1
that are contained in s2
.
Remarks
This function stops searching when a character from s1
is
not in s2
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <string.h>
#include <stdio.h>
int main(void)
{
char str1[20] = "animal";
char str2[20] = "aeiounm";
char str3[20] = "aimnl";
char str4[20] = "xyz";
int res;
res = strspn(str1, str2);
printf("strspn(\"%s\", \"%s\") = %d\n",
str1, str2, res);
res = strspn(str1, str3);
printf("strspn(\"%s\", \"%s\") = %d\n",
str1, str3, res);
res = strspn(str1, str4);
printf("strspn(\"%s\", \"%s\") = %d\n",
str1, str4, res);
}
Example Output
strspn("animal", "aeiounm") = 5
strspn("animal", "aimnl") = 6
strspn("animal", "xyz") = 0
Example Explanation
In the first result, l
is not in s2
.
In the second result, the terminating null is not in s2
.
In the third result, a
is not in s2
, so
the comparison stops.