Calculates the gamma function of a single precision floating-point argument.
Include
<math.h>
Prototype
float tgammaf(float x);
Argument
x |
Return Value
Calculates the gamma function of the argument.
Remarks
If x
is negative or if the result cannot be represented with
x
is zero, a domain error will occur and errno
will be set to EDOM
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
float x, y;
x = 0.5;
y = tgammaf(x);
if(errno)
perror("Error");
printf("The gamma function of %f is %f\n", x, y);
x = -0.75;
y = tgammaf(x);
if(errno)
perror("Error");
printf("The gamma function of %f is %f\n", x, y);
}
Example Output
The gamma function of 0.500000 is 1.772454
The gamma function of -0.750000 is -4.834147