Prints formatted data to a wide character array using a wide format string and variable length argument list.
Include
<wchar.h>
Prototype
int vswprintf(wchar_t * restrict s, size_t n, const wchar_t * restrict
format, va_list arg);
Arguments
s | |
n | |
format | |
arg |
Return Value
Returns number of characters generated or a negative number if an error occurs.
Remarks
The function writes formatted output to the specified wide character array.
The format
string is composed of text, which is copied unchanged to
the output stream, and conversion specifications, which begin with the
%
wide character and which fetch zero or more of the optional
arguments, converting them according to the corresponding conversion specifier when
required, and then writing the result to the output stream. If the are less
arguments than required by the conversion specifications, the output is undefined.
If there are more arguments than required by the conversion specifications, the
additional arguments are unused.
Each conversion specification begins with a percent sign followed by optional fields and a required type as shown here:
%[flags][width][.precision][length]specifier
The flags
modify the meaning of the conversion
specification. The are described in the following table.
Flag | Meaning |
---|---|
- |
Left justify the conversion result within a given field width. |
0 |
Use 0 for the pad character instead of
space (which is the default) for d ,
i , o , u ,
x , X , a ,
A , e,
E , f , F ,
g , and G conversions, except
when converting an infinity or NaN. If the 0 and
- flags both appear, the 0
flag is ignored. For d , i ,
o , u , x ,
andX conversions, if a precision is specified,
the 0 flag is ignored. For other conversions, the
behavior is undefined. |
+ |
Write a plus sign for positive signed conversion results. |
space | Prefix a space when the first wide
character of a conversion result does not include a sign
(+ or - ) or if a signed
conversion results in no wide characters. If the space and
+ flags both appear, the space flag is
ignored. |
# |
Convert the result to an alternative form.
Specifically, for o conversions, it increases the
precision, ensuring the first digit of the result is a zero, if and
only if necessary. (If the value and precision are both 0, a single
0 is printed). For x (or X )
conversions, 0x (or 0X ) is
prefixed to nonzero results. For a ,
A , e , E ,
f , F , g , and
G conversions, the result of converting a
floating-point number always contains a decimal-point wide
character, even if no digits follow it. For g and
G conversions, trailing zeros are not removed
from the result. For other conversions, the behavior is
undefined. |
The width
field indicated how many characters the
value should consume. If the converted value has fewer characters than the field
width, it is padded with spaces on the left, unless the left adjustment flag
-
has been used.
If the asterisk, *
, is used instead of a decimal number, the
int
argument before the argument to be converted will be used
for the field width. If the result is less than the field width, pad characters will
be used on the left to fill the field. If the result is greater than the field
width, the field is expanded to accommodate the value without padding.
precision
field indicates:d
, i
,
o
, u
, x
, and
X
conversionsa
,
A
, e
, E
,
f
, and F
conversionsg
and G
conversionss
conversions.
, followed either
by an asterisk, *
or by an optional decimal integer. If neither the
*
or integer is specified, the precision is assumed to be zero.
If the asterisk, *
, is used instead of a decimal number, the
int
argument before the argument to be converted will be used
for the precision. If a precision appears with any other conversion specifier, the
behavior is undefined.The length
modifier specifies the size of the
argument as described in the following table. Their use with other conversion
specifiers results in undefined behavior.
Modifier | Meaning |
---|---|
h |
When used with d ,
i , o , u ,
x , or X conversion specifiers,
converts the argument value to a short int or
unsigned short int . |
h |
When used with the n
conversion specifier, indicates that the pointer argument points to
a short int . |
hh |
When used with d ,
i , o , u ,
x , or X conversion specifiers,
converts the argument value to a signed char or
unsigned char . |
j |
When used with d ,
i , o , u ,
x , or X conversion specifiers,
indicates that the argument value is aintmax_t or
uintmax_t . |
j |
When used with the n
conversion specifier, indicates that the pointer points to a
intmax_t . |
l |
When used with d ,
i , o , u ,
x , or X conversion specifiers,
converts the argument value to a long int or
unsigned long int . |
l |
When used with the n
conversion specifier, indicates that the pointer points to a
long int . |
l |
When used with the c
conversion specifier, indicates that the argument value is a wide
character (wint_t type). |
l |
When used with the s
conversion specifier, indicates that the argument value is a wide
string (wchar_t type). |
l |
When used the e ,
E , f , F ,
g , G , has no effect. |
ll |
When used with d ,
i , o , u ,
x , or X conversion specifiers,
indicates that the argument value is a long long
int or unsigned long long int . |
ll |
When used with the n
conversion specifier, indicates that the pointer points to a
long long int . |
ll |
MPLAB XC16: When used with the Other compilers: The modifier is silently ignored. |
L |
When used the a ,
A , e , E ,
f , F , g ,
G conversion specifier, indicates the argument
value is a long double . |
t |
When used with d ,
i , o , u ,
x , or X conversion specifiers,
indicates that the argument value is a ptrdiff_t or
the corresponding unsigned integer type. |
t |
When used with the n
conversion specifier, indicates that the pointer points to a
ptrdiff_t . |
z |
When used with d ,
i , o , u ,
x , or X conversion specifiers,
indicates that the argument value is a size_t_t or
the corresponding signed integer type. |
z |
When used with the n
conversion specifier, indicates that the pointer points to a
size_t_t . |
The conversion specifiers
specify the type of
conversion to be applied to the argument and how that value should be printed, as
described in the following table.
Specifier | Argument value type | Printing notes |
---|---|---|
a ,
A |
double |
Converted to the general form
[−]0xh.hhhhp±d ,
where there is one hexadecimal digit before the decimal-point wide
character and the number of hexadecimal digits after it is equal to
the precision. |
c |
char or wint_t |
The integer argument value is converted to a wide character (as if by calling btowc) and the resulting wide character is written. When the |
d |
signed int |
Converted to signed decimal with the
general form [−]dddd . The
precision specifies the minimum number of digits to appear. |
e , E |
double |
Converted to the general form
[−]d.ddde±dd ,
where there is one digit before the decimal-point wide character and
the number of digits after it is equal to the precision, which is 6
if that is missing. If the precision is zero and the
# flag is not specified, no decimal-point wide
character appears. |
f ,
F |
double |
Converted to decimal notation using the
general form
[−]ddd.ddd ,
where the number of digits after the decimal-point character is
equal to the precision specification, which is 6 if that is missing.
If the precision is zero and the # flag is not
specified, no decimal-point wide character appears. |
g , G |
double |
takes the form of e ,
f , or E or F
in the case of G , as appropriate |
i |
signed int |
Converted to signed decimal with the
general form [−]dddd . The
precision specifies the minimum number of digits to appear. |
n |
an integer pointer | The number of wide characters written so far is written to the object pointed to by the pointer. No wide characters are printed. |
o |
unsigned int |
Converted to unsigned octal with the
general form dddd . The precision
specifies the minimum number of digits to appear |
p |
void * |
Printed as the value (address) held by the pointer. |
s |
char array, or wchar_t
array |
A string contain multibyte characters that are converted to wide
characters (as if by calling When the |
u |
unsigned int |
Converted to unsigned decimal with the
general form dddd . The precision
specifies the minimum number of digits to appear |
x |
unsigned int |
Converted to unsigned hexadecimal notation
with the general form dddd . The
letters abcdef are printed for digits above 9. The
precision specifies the minimum number of digits to appear |
X |
unsigned int |
Converted to unsigned hexadecimal notation
with the general form dddd . The
letters ABCDEF are printed for digits above 9. The
precision specifies the minimum number of digits to appear |
% |
No argument is converted and a
% wide character is printed. |
Example
#include <wchar.h>
#include <stdarg.h>
int prWstr(wchar_t * ws, const wchar_t * fmt, ...)
{
va_list ap;
int n;
va_start(ap, fmt);
n = vswprintf(ws, 30, fmt, ap);
va_end(ap);
return n;
}
wchar_t wbuf[30];
int main(void)
{
int y;
wchar_t s[] = L"Print this string";
int x = 1;
wchar_t a = L'\n';
y = prWstr(wbuf, L"%ls %d time%lc", s, x, a);
printf("Number of characters printed to wide string buffer = %d\n", y);
}
Example Output
Number of characters printed to wide string buffer = 25