Converts calendar time to a string representation of local time.
Include
<time.h>
Prototype
char *ctime(const time_t *tod);
Argument
tod |
Return Value
Returns the address of a string that represents the local time of the parameter passed.
Remarks
This function is equivalent to asctime(localtime(tod))
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <time.h>
#include <stdio.h>
int main(void)
{
time_t whattime;
struct tm nowtime;
nowtime.tm_sec = 30;
nowtime.tm_min = 30;
nowtime.tm_hour = 2;
nowtime.tm_mday = 1;
nowtime.tm_mon = 1;
nowtime.tm_year = 103;
whattime = mktime(&nowtime);
printf("Day and time %s\n", ctime(&whattime));
}
Example Output
Day and time Sat Feb 1 02:30:30 2003