Calculates the base-2 logarithm of a long double-precision floating-point value.
Include
<math.h>
Prototype
long double log2l(long double x);
Argument
x |
Return Value
Returns the base-2 logarithm of x
. If x
is +/-0,
-infinity is returned. If x
is < 0, NaN is returned .
Remarks
If x
is less than 0, a domain error will occur and errno
will be set to EDOM
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
double x, y;
errno = 0;
x = 2.0;
y = log2l(x);
if(errno)
perror("Error");
printf("The base-2 logarithm of %Lf is %Lf\n", x, y);
errno = 0;
x = 0.0;
y = log2l(x);
if(errno)
perror("Error");
printf("The base-2 logarithm of %Lf is %Lf\n", x, y);
errno = 0;
x = -2.0;
y = log2l(x);
if(errno)
perror("Error");
printf("The base-2 logarithm of %Lf is %Lf\n", x, y);
}
Example Output
The base-2 logarithm of 2.000000 is 1.000000
The base-2 logarithm of 0.000000 is -inf
Error: domain error
The base-2 logarithm of -2.000000 is nan