Write data to a file.
Include
<unistd.h>
Prototype
int write(int handle, void * buffer, size_t
count);
Arguments
handle | |
buffer | |
count |
Return Value
If successful, write returns the number of characters actually written. A return value of
-1 indicates an error, in which case errno
should be set to indicate
the type of error. Suitable values may be EBADF
or
EINVAL
, among others.
Remarks
This function is implemented as a stub that must be completed to suite the application.
This is a helper function called by the Standard C Library function
fflush()
.
If the actual space remaining on the disk is less than the size of the buffer, the function trying to write to the disk write fails and does not flush any of the buffer’s contents to the disk. If the file is opened in text mode, each linefeed character is replaced with a carriage return-linefeed pair in the output. The replacement does not affect the return value.
Default Behavior
As distributed, the parameters are passed to the host file system through the simulator. The return value is the value returned by the host file system.
Source File
write.c