Obtains wide character input from a stream.
Include
<wchar.h>
Prototype
int getwc(FILE * stream);
Arguments
stream |
Return Value
Returns the next available wide character as a wchar_t
converted to a
wint_t
. The WEOF
wide character is returned if the
end-of-file indicator for the stream is set, if the stream is at end-of-file, if a read error
occurs, or if an encoding error occurs.
Remarks
The getwc()
function is equivalent to fgetwc()
. It is
implemented as a XXXX in MPLAB XC16 and XC32 (, hence it may evaluate stream more than
once.)
Example
#include <wchar.h>
int main(void)
{
FILE * myfile;
wint_t wc;
if ((myfile = fopen("afile", "r")) == NULL)
wprintf(L"Cannot open afile\n");
else
{
while( ! feof(myfile)) {
wc = getwc(myfile);
if(iswprint(wc))
wprintf(L"char read: %lc\n", wc);
}
fclose(myfile);
}
}
Example Input
Content of afile
.
Four score
Example Output
char read: F
char read: o
char read: u
char read: r
char read:
char read: s
char read: c
char read: o
char read: r
char read: e