Calculates the argument of a single precision complex value.
Include
<complex.h>
Prototype
float complex cargf(float complex z);
Argument
z |
Return Value
Returns the argument (or phase angle) of z
in the interval
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
float complex x, y;
x = -2.0 + 1.0*I;
y = cargf(x);
printf("The complex argument of %f + %fi is %f + %fi\n", crealf(x), cimagf(x), crealf(y), cimagf(y));
}
Example Output
The complex argument of -2.000000 + 1.000000i is 2.677945 + 0.000000i