Returns the long double precision floating-point argument rounded to an integer value.
Include
<math.h>
Prototype
long double rintl(long double x);
Argument
x |
Return Value
Returns the value of x
rounded to an integer value using the current
rounding direction, raising the inexact floating-point exception should the result not
have the same value as the argument. The rounded integer is returned as a long double
precision floating-point value.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
long double x, y;
x = 10.103;
y = rintl(x);
printf("The nearest integer value to %Lf is %Lf\n", x, y);
x = 10.51;
y = rintl(x);
printf("The nearest integer value to %Lf is %Lf\n", x, y);
}
Example Output
The nearest integer value to 10.103000 is 10.000000
The nearest integer value to 10.510000 is 11.000000