Performs a binary search.
Include
<stdlib.h>
Prototype
void *bsearch(const void *key, const void
*base, size_t nelem, size_t size, int
(*cmp)(const void *ck, const void
*ce));
Arguments
key | |
base | |
nelem | |
size | |
cmp |
Arguments to the comparison function are as follows.
ck | |
ce |
Return Value
Returns a pointer to the object being searched for if
found; otherwise, returns NULL
.
Remarks
The value returned by the compare function is <0 if
ck
is less than ce
, 0 if
ck
is equal to ce
or >0 if
ck
is greater than ce
.
In the following example, qsort
is used
to sort the list before bsearch
is called.
bsearch
requires the list to be sorted
according to the comparison function. This comp
uses ascending order.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <stdlib.h>
#include <stdio.h>
#define NUM 7
int comp(const void *e1, const void *e2);
int main(void)
{
int list[NUM] = {35, 47, 63, 25, 93, 16, 52};
int x, y;
int *r;
qsort(list, NUM, sizeof(int), comp);
printf("Sorted List: ");
for (x = 0; x < NUM; x++)
printf("%d ", list[x]);
y = 25;
r = bsearch(&y, list, NUM, sizeof(int), comp);
if (r)
printf("\nThe value %d was found\n", y);
else
printf("\nThe value %d was not found\n", y);
y = 75;
r = bsearch(&y, list, NUM, sizeof(int), comp);
if (r)
printf("\nThe value %d was found\n", y);
else
printf("\nThe value %d was not found\n", y);
}
int comp(const void *e1, const void *e2)
{
const int * a1 = e1;
const int * a2 = e2;
if (*a1 < *a2)
return -1;
else if (*a1 == *a2)
return 0;
else
return 1;
}
Example Output
Sorted List: 16 25 35 47 52 63 93
The value 25 was found
The value 75 was not found