The header file stdarg.h
supports functions with variable argument lists.
Variable argument lists allow functions to have an arbitrary number of arguments without corresponding parameter declarations, thus, the number and type of these arguments can differ on each call to the function.
A function with a variable argument list must have at least one named
argument. The arguments in the argument list are represented by
an ellipsis, ...
. To read the argument list, an
object of type va_list
must be declared inside
the function to hold information about the argument list. The
va_start
macro is used to
initialize the va_list
object so that the
argument values can be obtained, the va_arg
macro will access the next argument in the list, and the
va_end
macro ensures that the
function is in a state whereby it can successfully return after
all the required arguments have been read.