Determines if its first argument is smaller than its second.
Include
<math.h>
Prototype
int isless(floating-point x, floating-point
y);
Argument
x | |
y |
Return Value
Determines if x
is smaller than y
, as if by the
expression (x) < (y)
only without any invalid floating-point
exception should the arguments be unordered (i.e. should one of them be NaN).
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
double x, y;
int b;
x = -5.7;
y = 2.0;
b = isless(x, y);
printf("That %f is less than %f is %s\n", x, y, b ? "true" : "false");
}
Example Output
That -5.700000 is less than 2.000000 is true