Converts a multibyte character sequence to a wide string.
Include
<stdlib.h>
Prototype
size_t mbstowcs(wchar_t * restrict pwcs, const char * restrict s, size_t
n);
Arguments
pwcs | |
s | |
n |
Return Value
The function returns the number of wide characters, not including the terminating null
character (if any), stored to pwcs
. If s
cannot be
converted, (size_t)(-1)
is returned.
Remarks
The function converts a sequence of multibyte characters in the array s
and
that begins in the initial shift state into a sequence of corresponding wide characters,
storing no more than n
converted wide characters (including a terminating
null wide character) into the array pointed to by pwcs
. Conversion stops when
a terminating null character is encountered, when an invalid multibyte character sequence is
encountered, or when n
wide characters have been stored. Each conversion
takes place as if by a call to the mbtowc()
function, except that the
conversion state of the mbtowc()
function is not affected.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <locale.h>
#include <stdlib.h>
#include <wchar.h>
void printWide(const char * mbstr)
{
size_t len;
wchar_t wstr[40];
len = mbstowcs(wstr, mbstr, 40);
wprintf(L"Converted wide string \"%ls\" has length %u\n", wstr, len);
}
int main(void)
{
setlocale(LC_CTYPE, "");
printWide("It is 75°F");
}
Example Output
Converted wide string "It is 75°F" has length 10