Dynamically allocate a block of memory from the heap.
Include
<stdlib.h>
Prototype
void * malloc(size_t size);
Argument
size |
Return Value
Returns a pointer to the allocated memory if successful; otherwise, returns a null pointer.
Remarks
Although the memory block allocated and whose address is returned will be large enough to hold an object with the specified size, the memory required to allocate that block might be larger than the requested size due to alignment of the allocated memory, and/or additional objects that are used to manage the heap.
Unlike calloc
, the malloc
function does not initialize the
memory it allocates.
See your MPLAB XC compiler User's Guide for more information on dynamic memory allocation.
Example
#include <stdio.h>
#include <stdlib.h>
int main(void)
{
long *i;
if ((i = (long *)malloc(50 * sizeof(long))) == NULL)
printf("Cannot allocate memory\n");
else
{
printf("Memory allocated\n");
free(i);
printf("Memory freed\n");
}
}
Example Output
Memory allocated
Memory freed