Calculate the number of consecutive characters at the beginning of a string that are not contained in a set of characters.
Include
<string.h>
Prototype
size_t strcspn(const char *s1, const char
*s2);
Arguments
s1 | |
s2 |
Return Value
Returns the length of the segment in s1
not containing
characters found in s2
.
Remarks
This function will determine the number of consecutive characters from the
beginning of s1
that are not contained in s2
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <string.h>
#include <stdio.h>
int main(void)
{
char str1[20] = "hello";
char str2[20] = "aeiou";
char str3[20] = "animal";
char str4[20] = "xyz";
int res;
res = strcspn(str1, str2);
printf("strcspn(\"%s\", \"%s\") = %d\n",
str1, str2, res);
res = strcspn(str3, str2);
printf("strcspn(\"%s\", \"%s\") = %d\n",
str3, str2, res);
res = strcspn(str3, str4);
printf("strcspn(\"%s\", \"%s\") = %d\n",
str3, str4, res);
}
Example Output
strcspn("hello", "aeiou") = 1
strcspn("animal", "aeiou") = 0
strcspn("animal", "xyz") = 6
Example Explanation
In the first result, e
is in s2
so it stops
counting after h
.
In the second result, a
is in s2
.
In the third result, none of the characters of s1
are in
s2
so all characters are counted.