Determines the state of a specified subset of the currently set floating-point exceptions.
Include
<fenv.h>
Prototype
int fetestexcept(int excepts);
Argument
excepts |
Retrun Value
The function returns the bitwise OR of the floating-point exception macro values associated with those exceptions that are specified by the argument and that are currently set.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <fenv.h>
#include <stdio.h>
#include <math.h>
void showExceptions(void)
{
printf("Exceptions currently raised: ");
if(fetestexcept(FE_DIVBYZERO))
printf("FE_DIVBYZERO ");
if(fetestexcept(FE_INEXACT))
printf("FE_INEXACT ");
if(fetestexcept(FE_INVALID))
printf("FE_INVALID ");
if(fetestexcept(FE_OVERFLOW))
printf("FE_OVERFLOW ");
if(fetestexcept(FE_UNDERFLOW))
printf("FE_UNDERFLOW ");
printf("\n");
}
volatile double result = 0.0;
int main(void)
{
fexcept_t excepts;
result = 1.0 / result; // raise FE_DIVBYZERO
showExceptions();
fegetexceptflag(&excepts, FE_ALL_EXCEPT); // save state
feraiseexcept(FE_INVALID|FE_OVERFLOW); // raise exceptions without operation
showExceptions();
fesetexceptflag(&excepts, FE_ALL_EXCEPT); // restore state
showExceptions();
}
Example Output
Exceptions currently raised: FE_DIVBYZERO
Exceptions currently raised: FE_DIVBYZERO FE_INEXACT FE_INVALID FE_OVERFLOW
Exceptions currently raised: FE_DIVBYZERO