Sets the floating-point status flags to those represented by the state stored in the object.
Include
<fenv.h>
Prototype
void fesetexceptflag(fexcept_t * flagp, int excepts);
Arguments
flagp | |
excepts |
Remarks
The pointer must hold an address obtained by a previous call to
fegetexceptflag()
whose second argument represented
at least those floating-point exceptions being set by this call. Only those
state flags in the second argument may be set by this function. This
function does not raise floating-point exceptions; it only sets the state of
the flags.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <fenv.h>
#include <stdio.h>
#include <math.h>
void showExceptions(void)
{
printf("Exceptions currently raised: ");
if(fetestexcept(FE_DIVBYZERO))
printf("FE_DIVBYZERO ");
if(fetestexcept(FE_INEXACT))
printf("FE_INEXACT ");
if(fetestexcept(FE_INVALID))
printf("FE_INVALID ");
if(fetestexcept(FE_OVERFLOW))
printf("FE_OVERFLOW ");
if(fetestexcept(FE_UNDERFLOW))
printf("FE_UNDERFLOW ");
printf("\n");
}
volatile double result = 0.0;
int main(void)
{
fexcept_t excepts;
result = 1.0 / result; // raise FE_DIVBYZERO
showExceptions();
fegetexceptflag(&excepts, FE_ALL_EXCEPT); // save state
feraiseexcept(FE_INVALID|FE_OVERFLOW); // raise exceptions without operation
showExceptions();
fesetexceptflag(&excepts, FE_ALL_EXCEPT); // restore state
showExceptions();
}
Example Output
Exceptions currently raised: FE_DIVBYZERO
Exceptions currently raised: FE_DIVBYZERO FE_INEXACT FE_INVALID FE_OVERFLOW
Exceptions currently raised: FE_DIVBYZERO