Returns the long double precision floating-point argument rounded to the nearest integer value.
Include
<math.h>
Prototype
long long int llrintl(long double x);
Argument
x |
Return Value
Returns the value of x
rounded to the nearest integer value using the
current rounding direction. The rounded valued is returned as a long
long
integer value, but is unspecified if the rounded value is outside the
range of the return type.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
long double x;
long long int y;
x = 10.103;
y = llrintl(x);
printf("The nearest integer value to %Lf is %lld\n", x, y);
x = 10.51;
y = llrintl(x);
printf("The nearest integer value to %Lf is %lld\n", x, y);
}
Example Output
The nearest integer value to 10.103000 is 10
The nearest integer value to 10.510000 is 11