Search a string for the first occurrence of a character from a specified set of characters.
Include
<string.h>
Prototype
char *strpbrk(const char *s1, const char
*s2);
Arguments
s1 | |
s2 |
Return Value
Returns a pointer to the matched character in s1
if found;
otherwise, returns a null pointer.
Remarks
This function will search s1
for the first occurrence of a
character contained in s2
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <string.h>
#include <stdio.h>
int main(void)
{
char str1[20] = "What time is it?";
char str2[20] = "xyz";
char str3[20] = "eou?";
char *ptr;
int res;
printf("strpbrk(\"%s\", \"%s\")\n", str1, str2);
ptr = strpbrk(str1, str2);
if (ptr != NULL)
{
res = ptr - str1 + 1;
printf("match found at position %d\n", res);
}
else
printf("match not found\n");
printf("\n");
printf("strpbrk(\"%s\", \"%s\")\n", str1, str3);
ptr = strpbrk(str1, str3);
if (ptr != NULL)
{
res = ptr - str1 + 1;
printf("match found at position %d\n", res);
}
else
printf("match not found\n");
}
Example Output
strpbrk("What time is it?", "xyz")
match not found
strpbrk("What time is it?", "eou?")
match found at position 9