The following points relate to the general usage of functions within the library.
With the MPLAB XC8 compiler (for both PIC and AVR targets), the
double
and long double
types are the same size
and format as the 32-bit float
type. Many math-related functions
have separate implementations for each of the three floating-point types (e.g.
acos
for double
types, acosl
for long double
types, and acosf
for
float
types). In these cases, only the float
instance of the function is fully implemented. Calls to either the
double
or long double
variants of the
functions will be mapped to the float
implementation.
By default, the MPLAB XC16 compiler uses a double
type equivalent to
float
, which is 32 bit wide. The
-fno-short-double
option makes double
equivalent to long double
, which is 64 bit wide. The
characteristics of floating-point numbers, described in <float.h> Floating-Point Characteristics, change with
the use of this option, as indicated.
The MPLAB XC8 Compiler for AVR can store objects qualified const
into program memory (rather than data memory) and allow pointers to
const
types to access such objects. The feature is only
available for some devices and is enabled using the
-mconst-data-in-progmem
option. When enabled, pointers to a
const
-qualified type are treated differently to similar
pointers without the const
qualifier, so for example the addresses
held by pointers of type char *
and const char *
are interpreted as belonging to different address spaces.
const
-qualified type becomes a
const
-qualified version of that type. For example, with the
-mconst-data-in-progmem
option specified, the prototype for the
strtof
function, which is specified in the C standard
as:float strtof(const char * __restrict, char ** __restrict);
becomes:float strtof(const char * __restrict, const char ** __restrict);
This
change might affect how your program should be defined.