Calculates the natural logarithm of the absolute value of gamma of the single-precision floating-point argument.
Include
<math.h>
Prototype
float lgammaf(float x);
Argument
x |
Return Value
Returns the natural logarithm of the absolute value of gamma of the argument.
Remarks
A range error occurs if x
is too large, and errno
will
be set to ERANGE
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
float x, y;
x = 0.5;
y = lgammaf(x);
if(errno)
perror("Error");
printf("The natural log of gamma of %f is %f\n", x, y);
x = -0.75;
y = lgammaf(x);
if(errno)
perror("Error");
printf("The natural log of gamma of %f is %f\n", x, y);
}
Example Output
The natural log of gamma of 0.500000 is 0.572365
The natural log of gamma of -0.750000 is 1.575705