Test for a lowercase alphabetic character.
Include
<ctype.h>
Prototype
int islower (int c);
Argument
c |
Return Value
Returns a non-zero integer value if the character,
c
, is a lowercase alphabetic character;
otherwise, returns zero.
Remarks
A character is considered to be a lowercase alphabetic character if it is in the range of
'a'
-'z'
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <ctype.h>
#include <stdio.h>
int main(void)
{
int ch;
ch = 'B';
if (islower(ch))
printf("B is lowercase\n");
else
printf("B is NOT lowercase\n");
ch = 'b';
if (islower(ch))
printf("b is lowercase\n");
else
printf("b is NOT lowercase\n");
}
Example Output
B is NOT lowercase
b is lowercase