Obtains wide character input from a stream.
Include
<wchar.h>
Prototype
int fgetwc(FILE * stream);
Arguments
stream |
Return Value
Returns the next available wide character as a wchar_t
converted to a
wint_t
. The WEOF
wide character is returned if the
end-of-file indicator for the stream is set, if the stream is at end-of-file, if a read error
occurs, or if an encoding error occurs.
Remarks
This function advances the associated file position indicator for the stream (if defined) and
sets the end-of file indicator when the end-of-file is reached. If a read error occurs, the
error indicator for the stream is set and can be checked with the ferror()
function. If an encoding error occurs (which includes too few bytes), errno
is set to the value of the EILSEQ
macro.
Example
#include <wchar.h>
int main(void)
{
FILE * myfile;
wint_t wc;
if ((myfile = fopen("afile", "r")) == NULL)
wprintf(L"Cannot open afile\n");
else
{
while( ! feof(myfile)) {
wc = fgetwc(myfile);
if(iswprint(wc))
wprintf(L"char read: %lc\n", wc);
}
fclose(myfile);
}
}
Example Input
Content of afile
.
Four score
Example Output
char read: F
char read: o
char read: u
char read: r
char read:
char read: s
char read: c
char read: o
char read: r
char read: e