Calculates the base 2 exponential function of x
(2x
, where x
is a long double
precision floating-point value).
Include
<math.h>
Prototype
long double exp2l(long double x);
Argument
x |
Return Value
Returns 2x
.
Remarks
A range error occurs if the magnitude of x
is too large, and
errno
will be set to ERANGE
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
long double x, y;
errno = 0;
x = 1.0;
y = exp2l(x);
if (errno)
perror("Error");
printf("The base 2 exponential of %Lf is %Lf\n", x, y);
errno = 0;
x = 10;
y = exp2l(x);
if (errno)
perror("Error");
printf("The base 2 exponential of %Lf is %Lf\n", x, y);
errno = 0;
x = -10;
y = exp2l(x);
if (errno)
perror("Error");
printf("The base 2 exponential of %Lf is %Lf\n", x, y);
}
Example Output
The base 2 exponential of 1.000000 is 2.000000
The base 2 exponential of 10.000000 is 1024.000000
The base 2 exponential of -10.000000 is 0.000977