Transforms a string using the locale-dependent rules.
Include
<string.h>
Prototype
size_t strxfrm(char * restrict s1, const char * restrict s2, size_t
n);
Arguments
s1 | |
s2 | |
n |
Return Value
Returns the length of the transformed string not including the terminating null
character. If n
is zero, the string is not transformed
(s1
may be a point null in this case) and the length of
s2
is returned.
Remarks
The function transforms a string such that if two transformed strings are compared using
strcmp
, the result would be the same as comparing the original
strings using the strcoll
function. As no locales other than the
"C"
locale are supported, the transformation is equivalent to
strcpy
, except that the length of the destination string is bounded
by n
-1.