Create a new file.
Include
<unistd.h>
Prototype
int link(const char * existing, const char * new);
Arguments
existing | |
new |
Return Value
Zero is returned to indicate success, and -1 is returned to indicate an error condition.
Remarks
This function is implemented as a stub that must be completed to suite the application.
This function is not provided by default. Its purpose, in a file system, is to create a
new filename, new
, which contains the same data as the file named
existing
. The errno
object should also be set on
error. This function is used by rename
.
Source File
link.c