vfscanf Function

Scans formatted data from a stream using a variable length argument list.

Attention: This function is not implemented by MPLAB XC8 for PIC MCUs. It is implemented by all other compilers, but MPLAB XC8 for AVR MCUs has limited support of data streams.

Include

<stdio.h>

Prototype

int vfscanf(FILE * restrict stream, const char * restrict format, va_list arg);

Arguments

stream
pointer to the open stream
format
format control string
arg
pointer to a list of arguments

Return Value

If an input failure occurs before any conversion. the function returns the value of the macro EOF; otherwise, it returns the number of input items assigned.

Remarks

To access the variable length argument list, the arg variable must be initialized by the macro va_start and may be reinitialized by additional calls to va_arg. This must be done before the vfscanf function is called. Invoke va_end after the function returns.

When using MPLAB XC16, this function requires a heap.

To reduce code size, the functionality of this routine can be customized with each build. See the Smart IO Routines section in your compiler's user's guide for more information.

The format string can be composed of white space characters, which reads input up to the first non-white-space character in the input; or ordinary multibyte characters, which if not read in that order, will trigger an error and leave the remaining characters in the input, unread. The format string can also contain conversion specifications, which begin with the % character and that specify the expected input sequences and how they are to be converted for assignment to objects pointed to by the pointer arguments.

Each conversion specification begins with a percent character followed by optional fields and a required type as shown here:

%[*][width][length]specifier

The presence of * immediately after the percent character indicates that the read and converted value should not be assigned to any object.

The width is a decimal integer that must be non-zero and indicates the maximum field width (in characters) of the input that is read to match the specification.

The length modifier specifies the size of the object in which the value will be assigned, as described in the following table. Their use with other conversion specifiers results in undefined behavior.

Modifier Meaning
h  When used with d, i, o, u, x, X, or n indicates that this conversion specifier assigns to a short int or unsigned short int object referenced by the pointer argument.
hh When used with d, i, o, u, x, X, or n indicates that this conversion specifier assigns to a signed char or unsigned char object referenced by the pointer argument.
l When used with d, i, o, u, x, X, or n indicates that this conversion specifier assigns to a long int or unsigned long int object referenced by the pointer argument.
l When used the a, A, e, E, f, F, g, or G indicates that this conversion specifier assigns to a double object referenced by the pointer argument.
l When used the c, s, or [ indicates that this conversion specifier assigns to a wchar_t object referenced by the pointer argument.
ll When used with d, i, o, u, x, X, or n indicates that this conversion specifier assigns to a long long int or unsigned long long int object referenced by the pointer argument.
L When used the a, A, e, E, f, F, g, G conversion specifier, indicates the argument value is a long double.
j When used with d, i, o, u, x, X, or n indicates that this conversion specifier assigns to a intmax_t or uintmax_t object referenced by the pointer argument.
t When used with d, i, o, u, x, X, or n indicates that this conversion specifier assigns to a ptrdiff_t object referenced by the pointer argument.
z When used with d, i, o, u, x, X, or n indicates that this conversion specifier assigns to a size_t object referenced by the pointer argument.

The conversion specifiers specify the type of conversion to be applied to the read sequence.

Specifier Receiving object type Matches
a double Matches an optionally signed floating-point number, infinity, or NaN, whose format is the same as expected by the strtod function for the first argument.
c char array, or wchar_t array Matches a single character or the number of characters specified by the field width if present. If an l length modifier is present, the input shall be a sequence of multibyte characters, converted to a wide character as if by a call to the mbrtowc function. No null character or wide character is added.
d signed int Matches an optionally signed decimal integer, whose format is the same as expected by the strtod function for the first argument when using a value of 10 for the base argument.
e double Matches an optionally signed floating-point number, infinity, or NaN, whose format is the same as expected by the strtod function for the first argument.
f double Matches an optionally signed floating-point number, infinity, or NaN, whose format is the same as expected by the strtod function for the first argument.
g double Matches an optionally signed floating-point number, infinity, or NaN, whose format is the same as expected by the strtod function for the first argument.
i signed int Matches an optionally signed decimal integer, whose format is the same as expected by the strtod function for the first argument when using a value of 0 for the base argument.
n int No input is consumed but the number of characters this call has so far read from the input stream is written to the argument with no increment of the assignment count returned by the function. If the conversion specification includes an assignment-suppressing character or a field width, the behavior is undefined.
o unsigned int Matches an optionally signed decimal integer, whose format is the same as expected by the strtoul function for the first argument when using a value of 8 for the base argument.
p void * * Matches an implementation-defined set of sequences, which should be the same as the set of sequences that may be produced by the %p conversion of the fprintf function. The input item is converted to a pointer value in an implementation-defined manner. If the input item is a value converted earlier during the same program execution, the pointer that results shall compare equal to that value; otherwise the behavior of the %p conversion is undefined.
s char array, or wchar_t array

Matches a sequences of non-white-space characters, which is written to the array argument and appended with a null terminating character. If an l length modifier is present, the input shall be a sequence of multibyte characters, converted to a wide character and terminated with a null wide character.

x unsigned int Matches an optionally signed decimal integer, whose format is the same as expected by the strtoul function for the first argument when using a value of 16 for the base argument.
%   Matches a single % character. No assignment takes place.
[ char array, or wchar_t array Matches all the characters in the input that have been specified between the [ and trailing ] character, unless the character after the opening bracket is a circumflex, ^, in which case a match is only made with characters that do not appear in the brackets. If the conversion specifier begins with [] or [^], the right bracket character will match the input and the next following right bracket character is the matching right bracket that ends the specification. A null character will be appended to the characters read. If an l length modifier is present, the input shall be a sequence of multibyte characters and a null wide character will be appended to the matched wide characters.

Example

#include <stdio.h>
#include <stdarg.h>

void readArgs(FILE * stream, const char * format, ...)
{
  va_list args;
  va_start(args, format);
  vfscanf(stream, format, args);
  va_end(args);
}

int main(void)
{
  FILE * myfile;
  int val;
  char str[20];

  myfile = fopen("afile", "r");

  if(myfile!=NULL) {
    readArgs( myfile, "%s %d", str, &val);
    printf("String and value read: %s and %d\n", str, val);
    fclose(myfile);
  }
}

Example Input

Contents of afile.txt


Start 23
Stop 0

Example Output

String and value read: Start and 23