Macros that specify the minimum and maximum limits of the types with fixed width declared
in <stdint.h>
.
Include
<stdint.h>
Remarks
Each macro name corresponds to the <stdint.h>
type with a similar
name. The macro will expand to a constant expression suitable for use in
#if
preprocessing directives, and this expression shall have the
same type as an object of the corresponding type converted according to the integer
promotions.
Type | Description |
---|---|
INT8_MIN |
Minimum value of signed integer with 8 bits width. |
INT8_MAX |
Maximum value of signed integer with 8 bits width. |
UINT8_MAX |
Maximum value of unsigned integer with 8 bits width. |
INT16_MIN |
Minimum value of signed integer with 16 bits width. |
INT16_MAX |
Maximum value of signed integer with 16 bits width. |
UINT16_MAX |
Maximum value of unsigned integer with 16 bits width. |
INT24_MIN |
Minimum value of signed integer with 24 bits width (see Attention note). |
INT24_MAX |
Maximum value of signed integer with 24 bits width (see Attention note). |
UINT24_MAX |
Maximum value of unsigned integer with 24 bits width (see Attention note). |
INT32_MIN |
Minimum value of signed integer with 32 bits width. |
INT32_MAX |
Maximum value of signed integer with 32 bits width. |
UINT32_MAX |
Maximum value of unsigned integer with 32 bits width. |
INT64_MIN |
Minimum value of signed integer with 64 bits width (see Attention note). |
INT64_MAX |
Maximum value of signed integer with 64 bits width (see Attention note). |
UINT64_MAX |
Maximum value of unsigned integer with 64 bits width (see Attention note). |