A type that can hold processor time values, as returned by the clock
function.
Include
<time.h>
Structure used to hold the components of a calendar time, called the broken-down time
Include
<time.h>
Definition
struct tm {
int tm_sec; /*seconds after the minute ( 0 to 61 )*/
/*allows for up to two leap seconds*/
int tm_min; /*minutes after the hour ( 0 to 59 )*/
int tm_hour; /*hours since midnight ( 0 to 23 )*/
int tm_mday; /*day of month ( 1 to 31 )*/
int tm_mon; /*month ( 0 to 11 where January = 0 )*/
int tm_year; /*years since 1900*/
int tm_wday; /*day of week ( 0 to 6 where Sunday = 0 )*/
int tm_yday; /*day of year ( 0 to 365 where January 1 = 0 )*/
int tm_isdst; /*Daylight Savings Time flag */
long __tm_gmtoff; /*number of seconds offset from UTC to get local time*/
const char *__tm_zone; /*name of the time zone*/
}
Remarks
If tm_isdst
is a positive value, Daylight Savings is in effect. If
it is zero, Daylight Saving Time is not in effect. If it is a negative value, the
status of Daylight Saving Time is not known.
A type that can hold calendar time values, as returned by the time
function.
Include
<time.h>