Calculates the complex base-
Include
<complex.h>
Prototype
double complex clog(double complex z);
Argument
z |
Return Value
Returns the complex base-
z
, with no bound
along the real axis, in the interval
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
double complex x, y;
x = -2.0 + 1.0*I;
y = clog(x);
printf("The complex base-e logarithm of %f + %fi is %f + %fi\n", creal(x), cimag(x), creal(y), cimag(y));
}
Example Output
The complex base-e logarithm of -2.000000 + 1.000000i is 0.804719 + 2.677945i