Calculates the trigonometric arc cosine function of a single precision floating-point value.
Include
<math.h>
Prototype
float acosf(float x);
Argument
x |
Return Value
Returns the arc cosine of x
in the range
Remarks
If x
is less than -1 or greater than 1, a domain error will occur and
errno
will be set to EDOM
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
float x, y;
errno = 0;
x = 2.0F;
y = acosf (x);
if (errno)
perror("Error");
printf("The arccosine of %f is %f\n", x, y);
errno = 0;
x = 0.0F;
y = acosf (x);
if (errno)
perror("Error");
printf("The arccosine of %f is %f\n", x, y);
}
Example Output
Error: Domain error
The arccosine of 2.000000 is nan
The arccosine of 0.000000 is 1.570796