Calculates the trigonometric arc tangent function of
y/x
.
Include
<math.h>
Prototype
float atan2f(float y, float x);
Arguments
y | |
x |
Return Value
Returns the arc tangent in radians in the range
Remarks
A domain error occurs if both x
and y
are zero.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
float x, y, z;
errno = 0;
x = 2.0F;
y = 0.0F;
z = atan2f (y, x);
if (errno)
perror("Error");
printf("The arctangent of %f/%f is %f\n", y, x, z);
errno = 0;
x = 0.0F;
y = -1.0F;
z = atan2f (y, x);
if (errno)
perror("Error");
printf("The arctangent of %f/%f is %f\n", y, x, z);
errno = 0;
x = 0.0F;
y = 0.0F;
z = atan2f (y, x);
if (errno)
perror("Error");
printf("The arctangent of %f/%f is %f\n", y, x, z);
}
Example Output
The arctangent of 2.000000/0.000000 is 1.570796
The arctangent of 0.000000/-1.000000 is 3.141593
Error: domain error
The arctangent of 0.000000/0.000000 is nan