Calculates the signed exponent of a double precision floating-point value.
Include
<math.h>
Prototype
double scalbn(double x, int n);
Arguments
x | |
n | FLT_RADIX is raised |
Return Value
Efficiently calculates and returns the value of x
times
FLT_RADIX
n
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
double x, y;
int power;
errno = 0;
x = 13.45;
power = 8;
y = scalbn(x, power);
if (errno)
perror("Error");
printf("FLT_RADIX raised to the power %d, times %f is %f\n", power, x, y);
}
Example Output
FLT_RADIX raised to the power 8, times 13.450000 is 3443.200000