Calculates the argument of a double precision complex value.
Include
<complex.h>
Prototype
double complex carg(double complex z);
Argument
z |
Return Value
Returns the argument (or phase angle) of z
in the interval
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
double complex x, y;
x = -2.0 + 1.0*I;
y = carg(x);
printf("The complex argument of %f + %fi is %f + %fi\n", creal(x), cimag(x), creal(y), cimag(y));
}
Example Output
The complex argument of -2.000000 + 1.000000i is 2.677945 + 0.000000i