Determines if its first argument is smaller than or equal to its second.
Include
<math.h>
Prototype
int islessequal(floating-point x, floating-point
y);
Argument
x | |
y |
Return Value
Determines if x
is smaller than or equal to y
, as if by
the expression (x) <= (y)
only without any invalid floating-point
exception should the arguments be unordered (i.e. should one of them be NaN).
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
double x, y;
int b;
x = -5.7;
y = 2.0;
b = islessequal(x, y);
printf("That %f is less than or equal to %f is %s\n", x, y, b ? "true" : "false");
}
Example Output
That -5.700000 is less than or equal to 2.000000 is true