Calculates the complex sine function of a single precision complex value.
Include
<complex.h>
Prototype
float complex csinf(float complex z);
Argument
z |
Return Value
Returns the complex sine of z
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
float complex x, y;
x = -2.0 + 1.0*I;
y = csinf(x);
printf("The complex sine of %f + %fi is %f + %fi\n", crealf(x), cimagf(x), crealf(y), cimagf(y));
}
Example Output
The complex sine of -2.000000 + 1.000000i is -1.403119 + -0.489056i