Returns a single precision value with the magnitude of one value and the sign of another.
Include
<math.h>
Prototype
float copysignf(float x, float y);
Arguments
x | |
y |
Return Value
Returns the value of x
but with the sign of
y
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
float x,y,z;
x = 10.0;
y = -3.0;
z = copysignf(x, y);
printf("The value %f but with %f's sign is %f\n\n", x, y, z);
}
Example Output
The value 10.000000 but with -3.000000's sign is -10.000000