Appends a copy of the source string to the end of the destination string.
Include
<string.h>
Prototype
char *strcat(char *s1, const char *s2);
Arguments
s1 | |
s2 |
Return Value
Returns a pointer to the destination string.
Remarks
This function appends the source string (including the terminating null character) to the end of the destination string. The initial character of the source string overwrites the null character at the end of the destination string. If the buffers overlap, the behavior is undefined.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <string.h>
#include <stdio.h>
int main(void)
{
char buf1[50] = "We're here";
char buf2[50] = "Where is the time?";
printf("buf1 : %s\n", buf1);
printf("\t(%d characters)\n\n", strlen(buf1));
printf("buf2 : %s\n", buf2);
printf("\t(%d characters)\n\n", strlen(buf2));
strcat(buf1, buf2);
printf("buf1 after strcat of buf2: \n\t%s\n",
buf1);
printf("\t(%d characters)\n", strlen(buf1));
printf("\n");
strcat(buf1, "Why?");
printf("buf1 after strcat of \"Why?\": \n\t%s\n",
buf1);
printf("\t(%d characters)\n", strlen(buf1));
}
Example Output
buf1 : We're here
(10 characters)
buf2 : Where is the time?
(18 characters)
buf1 after strcat of buf2:
We're hereWhere is the time?
(28 characters)
buf1 after strcat of "Why?":
We're hereWhere is the time?Why?
(32 characters)