Calculates the trigonometric cosine function of a long double precision floating-point value.
Include
<math.h>
Prototype
long double cosl(long double x);
Argument
x |
Return Value
Returns the cosine of x
specified in radians in the range
x
is
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
long double x,y;
errno = 0;
x = -1.0;
y = cosl(x);
if (errno)
perror("Error");
printf("The cosine of %Lf is %Lf\n", x, y);
errno = 0;
x = 0.0;
y = cosl(x);
if (errno)
perror("Error");
printf("The cosine of %Lf is %Lf\n", x, y);
}
Example Output
The cosine of -1.000000 is 0.540302
The cosine of 0.000000 is 1.000000