Calculates the complex base-
Include
<complex.h>
Prototype
double complex cexp(double complex z);
Argument
z |
Return Value
Returns the complex base-
z
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
double complex x, y;
x = -2.0 + 1.0*I;
y = cexp(x);
printf("The complex base-e exponential of %f + %fi is %f + %fi\n", creal(x), cimag(x), creal(y), cimag(y));
}
Example Output
The complex base-e exponential of -2.000000 + 1.000000i is 0.073122 + 0.113881i