Placeholder macros that can be used with the printf
family of functions
when printing signed integer values.
Include
<inttypes.h>
Remarks
The macros in following table expand to character string literals representing conversion
specifier characters that can be used with the printf
family of
functions when printing signed integer values.
Macro Name | Description |
---|---|
PRId8 |
Decimal placeholder string for a signed 8-bit
integer type (int8_t ). |
PRId16 |
Decimal placeholder string for a signed 16-bit
integer type (int16_t ). |
PRId32 |
Decimal placeholder string for a signed 32-bit
integer type (int32_t ). |
PRId64 |
Decimal placeholder string for a signed 64-bit
integer type (int64_t ), where supported (see Attention
note). |
PRIi8 |
Integer placeholder string for a signed 8-bit
integer type (int8_t ). |
PRIi16 |
Integer placeholder string for a signed 16-bit
integer type (int16_t ). |
PRIi32 |
Integer placeholder string for a signed 32-bit
integer type (int32_t ). |
PRIi64 |
Integer placeholder string for a signed 64-bit
integer type (int64_t ), where supported (see Attention
note). |
PRIdFAST8 |
Decimal placeholder string for the fastest
signed integer type with a width of at least 8 bits
(int_fast8_t ). |
PRIdFAST16 |
Decimal placeholder string for the fastest
signed integer type with a width of at least 16 bits
(int_fast16_t ). |
PRIdFAST32 |
Decimal placeholder string for the fastest
signed integer type with a width of at least 32 bits
(int_fast32_t ). |
PRIdFAST64 |
Decimal placeholder string for the fastest
signed integer type with a width of at least 64 bits
(int_fast64_t ), where supported (see Attention
note). |
PRIiFAST8 |
Integer placeholder string for the fastest
signed integer type with a width of at least 8 bits
(int_fast8_t ). |
PRIiFAST16 |
Integer placeholder string for the fastest
signed integer type with a width of at least 16 bits
(int_fast16_t ). |
PRIiFAST32 |
Integer placeholder string for the fastest
signed integer type with a width of at least 32 bits
(int_fast32_t ). |
PRIiFAST64 |
Integer placeholder string for the fastest
signed integer type with a width of at least 64 bits
(int_fast64_t ), where supported (see Attention
note). |
PRIdLEAST8 |
Decimal placeholder string for a signed integer
type with a width of at least 8 bits
(int_least8_t ). |
PRIdLEAST16 |
Decimal placeholder string for a signed integer
type with a width of at least 16 bits
(int_least16_t ). |
PRIdLEAST32 |
Decimal placeholder string for a signed integer
type with a width of at least 32 bits
(int_least32_t ). |
PRIdLEAST64 |
Decimal placeholder string for a signed integer
type with a width of at least 64 bits (int_least64_t ),
where supported (see Attention note). |
PRIiLEAST8 |
Integer placeholder string for a signed integer
type with a width of at least 8 bits
(int_least8_t ). |
PRIiLEAST16 |
Integer placeholder string for a signed integer
type with a width of at least 16 bits
(int_least16_t ). |
PRIiLEAST32 |
Integer placeholder string for a signed integer
type with a width of at least 32 bits
(int_least32_t ). |
PRIiLEAST64 |
Integer placeholder string for a signed integer
type with a width of at least 64 bits (int_least64_t ),
where supported (see Attention note). |
PRIdMAX |
Decimal placeholder string for a signed integer
type with maximum width (intmax_t ). |
PRIiMAX |
Integer placeholder string for a signed integer
type with maximum width (intmax_t ). |
PRIdPTR |
Decimal placeholder string for the
intptr_t type. |
PRIiPTR |
Integer placeholder string for the
intptr_t type. |
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <stdio.h>
#include <inttypes.h>
int8_t s8 = 23;
int_least32_t l32 = -324;
int main(void)
{
printf("s8 value: %" PRId8 "\n", s8);
printf("l32 value: %" PRIiLEAST32 "\n", l32);
}