llroundf Function

Returns the single precision floating-point argument rounded to an integer value.

Include

<math.h>

Prototype

long long int llroundf(float x);

Argument

x
the value to round

Return Value

Returns the value of x rounded to the nearest integer value, always rounding midway cases away from zero. The rounded value is returned as a long long integer value, but is unspecified should the rounded value fall outside the range of the return type.

Example

See the notes at the beginning of this chapter or section for information on using printf() or scanf() (and other functions reading and writing the stdin or stdout streams) in the example code.

#include <math.h>
#include <stdio.h>

int main(void)
{
  float x;
  long long int y;

  x = 10.103;
  y = llroundf(x);
  printf("The nearest integer value to %f is %lld\n", x, y);

  x = 10.5;
  y = llroundf(x);
  printf("The nearest integer value to %f is %lld\n", x, y);
}

Example Output

The nearest integer value to 10.103000 is 10
The nearest integer value to 10.500000 is 11