Determines the length of a multibyte character.
Include
<wchar.h>
Prototype
size_t mbrlen(const char * restrict s, size_t n, mbstate_t * restrict
ps);
Arguments
s | |
n | |
ps | mbstate_t object that holds the current conversion
state |
Return Value
The function returns the length of a multibyte sequence between 0 and n
inclusive, representing the length; or the value -1 or -2, as per the
mbrtowc()
function. nonzero if ps
is a null pointer or if
the pointed-to object describes an initial conversion state; otherwise, it returns zero.
Remarks
An object of type mbstate_t
is used to describe the current conversion state
from a particular multibyte character sequence to a wide character sequence (or the reverse
conversion) based on the current locale. For both conversions, the initial conversion state
corresponds to the beginning of a new multibyte character in the initial shift state. A
zero-valued mbstate_t
always represents an initial conversion state.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <wchar.h>
#include <stdlib.h>
#include <string.h>
int main(void)
{
char * string = "The final frontier";
mbstate_t state = {0};
wchar_t wc;
mbrtowc(&wc, string, MB_CUR_MAX, &state);
if(mbsinit(&state)) // check initial conversion state
wprintf(L"In initial conversion state\n");
else
memset(&state, 0, sizeof(state)); // set initial conversion state
}
Example Output
In initial conversion state