Converts a wide character string to a multibyte character sequence.
Include
<stdlib.h>
Prototype
size_t wcstombs(char * restrict s, const wchar_t * restrict pwcs, size_t
n);
Arguments
s | |
pwcs | |
n | s |
Return Value
The function returns the number of bytes in the multibyte character sequence, not including
the terminating null character (if any). If s
cannot be converted to a
mutlibyte character sequence, (size_t)(-1)
is returned.
Remarks
The function converts a wide character string indirectly pointed to by pwcs
beginning in the initial shift state into a sequence of corresponding multibyte characters,
storing no more than n
converted characters (including a terminating null
character) into the array pointed to by s
, provided dst
is
not a null pointer. Each conversion takes place as if by a call to the
wctomb()
function, except that the conversion state of the that function is
not affected.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <wchar.h>
#include <stdlib.h>
#include <locale.h>
int main(void) {
const wchar_t * ws = L"Volume: 2L±0.5mL";
char buffer[20];
size_t length;
setlocale(LC_CTYPE, "");
length = wcstombs(buffer, ws, 20);
wprintf(L"multibyte string \"%s\" has length %d\n", buffer, length);
}
Example Output
multibyte string "Volume: 2L±0.5mL" has length 17