Calculates the trigonometric sine function of a long double precision floating-point value.
Include
<math.h>
Prototype
long double sinl(long double x);
Argument
x |
Return Value
Returns the sine of x
specified in radians in the range
x
is
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
#include <errno.h>
int main(void)
{
long double x, y;
errno = 0;
x = -1.0;
y = sinl(x);
if (errno)
perror("Error");
printf("The sine of %Lf is %Lf\n", x, y);
errno = 0;
x = 0.0;
y = sinl(x);
if (errno)
perror("Error");
printf("The sine of %Lf is %Lf\n", x, y);
}
Example Output
The sine of -1.000000 is -0.841471
The sine of 0.000000 is 0.000000