Close a stream.
Include
<stdio.h>
Prototype
int fclose(FILE * stream);
Argument
stream |
Return Value
Returns 0 if successful; otherwise, returns EOF
if any errors were
detected.
Remarks
The fclose
function causes the stream indicated by the argument to be
flushed and the associated file to be closed. This function requires a heap.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <stdio.h>
int main(void)
{
FILE *myfile1, *myfile2;
int y;
if ((myfile1 = fopen("afile1", "w+")) == NULL)
printf("Cannot open afile1\n");
else
{
printf("afile1 was opened\n");
y = fclose(myfile1);
if (y == EOF)
printf("afile1 was not closed\n");
else
printf("afile1 was closed\n");
}
}
Example Output
afile1 was opened
afile1 was closed