Scans formatted text from a stream, using a wide format string.
Include
<wchar.h>
Prototype
int fwscanf(FILE * restrict stream, const wchar_t * restrict format,
...);
Arguments
stream | |
format | |
... |
Return Value
Returns the number of items successfully converted and assigned. If no items are
assigned, a 0 is returned. EOF
is returned if end-of-file is
encountered before the first conversion or if an error occurs.
Remarks
This function can read input from the specified stream.
The format
string can be composed of white space wide characters,
which reads input up to the first non-white-space wide character in the input; or
ordinary wide characters, which if not read in that order, will trigger an error and
leave the remaining characters in the input, unread. The format string can also
contain conversion specifications, which begin with the %
wide
character and that specify the expected input sequences and how they are to be
converted for assignment to objects pointed to by the pointer arguments.
Each conversion specification begins with a percent wide character followed by optional fields and a required type as shown here:
%[*][width][length]specifier
The presence of *
immediately after the percent wide character
indicates that the read and converted value should not be assigned to any
object.
The width
is a decimal integer that must be
non-zero and indicates the maximum field width (in characters) of the input that is
read to match the specification.
The length
modifier specifies the size of the
object in which the value will be assigned, as described in the following table.
Their use with other conversion specifiers results in undefined behavior.
Modifier | Meaning |
---|---|
h |
When used with d ,
i , o , u ,
x , X , or n
indicates that this conversion specifier assigns to a short
int or unsigned short int object
referenced by the pointer argument. |
hh |
When used with d ,
i , o , u ,
x , X , or n
indicates that this conversion specifier assigns to a signed
char or unsigned char object
referenced by the pointer argument. |
l |
When used with d ,
i , o , u ,
x , X , or n
indicates that this conversion specifier assigns to a long
int or unsigned long int object
referenced by the pointer argument. |
l |
When used the a ,
A , e , E ,
f , F , g , or
G indicates that this conversion specifier
assigns to a double object referenced by the
pointer argument. |
l |
When used the c ,
s , or [ indicates that this
conversion specifier assigns to a wchar_t object
referenced by the pointer argument. |
ll |
When used with d ,
i , o , u ,
x , X , or n
indicates that this conversion specifier assigns to a long
long int or unsigned long long int
object referenced by the pointer argument. |
L |
When used the a ,
A , e , E ,
f , F , g ,
G conversion specifier, indicates the argument
value is a long double . |
j |
When used with d ,
i , o , u ,
x , X , or n
indicates that this conversion specifier assigns to a
intmax_t or uintmax_t object
referenced by the pointer argument. |
t |
When used with d ,
i , o , u ,
x , X , or n
indicates that this conversion specifier assigns to a
ptrdiff_t object referenced by the pointer
argument. |
z |
When used with d ,
i , o , u ,
x , X , or n
indicates that this conversion specifier assigns to a
size_t object referenced by the pointer
argument. |
The conversion specifiers
specify the type of
conversion to be applied to the read sequence.
Specifier | Receiving object type | Matches |
---|---|---|
a |
double |
Matches an optionally signed floating-point
number, infinity, or NaN, whose format is the same as expected by
the strtod function for the first argument. |
c |
char array, or wchar_t
array |
Matches a single wide character or the number of characters specified by the field width if present. If no If an |
d |
signed int |
Matches an optionally signed decimal
integer, whose format is the same as expected by the
strtod function for the first argument when
using a value of 10 for the base argument. |
e |
double |
Matches an optionally signed floating-point
number, infinity, or NaN, whose format is the same as expected by
the strtod function for the first argument. |
f |
double |
Matches an optionally signed floating-point
number, infinity, or NaN, whose format is the same as expected by
the strtod function for the first argument. |
g |
double |
Matches an optionally signed floating-point
number, infinity, or NaN, whose format is the same as expected by
the strtod function for the first argument. |
i |
signed int |
Converted to signed decimal with the
general form [−]dddd . The
precision specifies the minimum number of digits to appear. |
n |
int |
No input is consumed but the number of wide characters this call has so far read from the input stream is written to the argument with no increment of the assignment count returned by the function. If the conversion specification includes an assignment-suppressing character or a field width, the behavior is undefined. |
o |
unsigned int |
Matches an optionally signed decimal
integer, whose format is the same as expected by the
strtoul function for the first argument when
using a value of 8 for the base argument. |
p |
void * * |
Matches an implementation-defined set of
sequences, which should be the same as the set of sequences that may
be produced by the %p conversion of the
fwprintf function. The input item is converted
to a pointer value in an implementation-defined manner. If the input
item is a value converted earlier during the same program execution,
the pointer that results shall compare equal to that value;
otherwise the behavior of the %p conversion is undefined. |
s |
char array, or wchar_t
array |
Matches a sequences of non-white-space wide characters, which is written to the array argument. If no If an |
x |
unsigned int |
Matches an optionally signed decimal
integer, whose format is the same as expected by the
strtoul function for the first argument when
using a value of 8 for the base argument. |
% |
Matches a single % wide
character. No assignment takes place. |
|
[ |
char array, or wchar_t
array |
Matches all the wide characters in the
input that have been specified between the l length modifier is
present, characters from the input field are converted to amultibyte
character sequence (as if by calling wcrtomb ). The
corresponding argument shall be a pointer to the initial element of
a character array large enough to accept the sequence and a
terminating null character, which will be added automatically.If
an |
Example
#include <wchar.h>
int main(void)
{
FILE *myfile;
wchar_t s[30];
int x;
wchar_t a;
if ((myfile = fopen("afile", "w+")) == NULL)
wprintf(L"Cannot open afile\n");
else
{
fwprintf(myfile, L"%ls %d times%lc", L"Print this string", 100, L'.');
fseek(myfile, 0L, SEEK_SET);
fwscanf(myfile, L"%ls", s);
wprintf(L"%ls\n", s);
fwscanf(myfile, L"%ls", s);
wprintf(L"%ls\n", s);
fwscanf(myfile, L"%ls", s);
wprintf(L"%ls\n", s);
fwscanf(myfile, L"%d", &x);
wprintf(L"%d\n", x);
fwscanf(myfile, L"%ls", s);
wprintf(L"%ls\n", s);
fclose(myfile);
}
}
Example Input
Contents of afile
:
Print this string 100 times.
Example Output
Print
this
string
100
times.