Break a wide string into tokens.
Include
<wchar.h>
Prototype
wchar_t * wcschr(wchar_t * restrict s1, const wchar_t * restrict s2,
wchar_t ** restrict ptr);
Arguments
s1 | |
s2 | |
ptr |
Return Value
Returns the address of the first element that matches the wide string if found; otherwise, returns a null pointer.
Remarks
This function will find the first occurrence of the wide string s2
(excluding the null terminator) within the string s1
. If s2
points to a zero length string, s1
is returned.
The address of the wide string to tokenize is passed as the first argument in a tokenizing
sequence. Subsequent calls should specify a null pointer as the first argument and the object
pointed to by ptr
is required to have the value stored by the previous call
in the sequence. The wide character string used as the delimiters may be different with each
call.
The first call in the sequence searches the wide string pointed to by s1
for
the first wide character that is not contained in the wide string pointed to by
s2
. If no match is found, and a null pointer is returned; otherwise this
wide character becomes the start of the first token.
If a wide character from the s2
wide string can be subsequently found from
the beginning of this token, it is replaced with a null wide character, thus correctly
terminating the token as a wide string. If no such wide character is found, the current token
extends to the end of the wide string pointed to by s1
.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <wchar.h>
int main(void)
{
wchar_t ws[] = L"- This, as they say, is the end.";
wchar_t * pwc;
wchar_t * ptr;
wprintf (L"\"%ls\" is tokenized:\n", ws);
pwc = wcstok (ws, L" ,.-", &ptr);
while (pwc != NULL)
{
wprintf (L"%ls\n", pwc);
pwc = wcstok (NULL, L" ,.-", &ptr);
}
}
Example Output
"- This, as they say, is the end." is tokenized:
This
as
they
say
is
the
end