Put a string to stdout
.
Include
<stdio.h>
Prototype
int puts(const char * s);
Argument
s |
Return Value
Returns a non-negative value if successful; otherwise, returns EOF
.
Remarks
The function writes characters to the stream stdout
. A newline character
is appended. The terminating null character is not written to the stream.
When building with the MPLAB XC8 compiler for PIC MCUs, the puts()
function relies on the putch()
function being properly defined to
direct output to the required peripheral or location. Printing will not work as expected
until the putch()
stub (found in the
pic/sources/c99/common/putch.c of your compiler distribution)
is completed. See Example code for 8-bit PIC MCUs
for information on defining putch()
so that printed text appears in an
MPLAB X IDE simulator window.
Example
#include <stdio.h>
int main(void)
{
char buf[] = "This is text\n";
puts(buf);
puts("|");
}
Example Output
This is text
|