Returns true if its argument is finite.
Include
<math.h>
Prototype
int isfinite(floating-point x);
Argument
x |
Return Value
Returns true if x
is finite, i.e. is not infinite or NaN.
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <math.h>
#include <stdio.h>
int main(void)
{
double x;
int b;
x = 0.0;
b = isfinite(x);
printf("The value %f is %sconsidered finite\n", x, b ? "" : "not ");
}
Example Output
The value 0.000000 is considered finite